AXIS#.IL.CMDACC

Description

Use AXIS#.IL.CMDACC to monitor the commanded acceleration for a given motion. This keyword is useful for tuning acceleration feedforward (AXIS#.IL.KACCFF).

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

Depends on AXIS#.UNIT.ACCROTARY .

Range

+/- 64bit

Default Value

0

Data Type

Float

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported.

Related Topics

AXIS#.IL.KACCFF | Tuning Fundamentals

Industrial Ethernet Information

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5822

1

5822 (0x16be)

AXIS1.IL.CMDACC

Signed32

Read Only

Yes

71358

2

5822 (0x16be)

AXIS2.IL.CMDACC

Signed32

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.IL.CMDACC

5822

Float

Read Only

Acceleration